Skip to main content
Associate II
Mar 20, 2025 7:10 AM UTC
Solved

Zigbee application stuck at M0 callback

Hi!
I am trying to reproduce some examples and got stuck at simple sensor.

The example code is working fine on my P-Nucleo-wb55, but if I am trying to reproduce i with CubeMX i've got failed

Code is simply stuck at 

void shci_cmd_resp_wait(uint32_t timeout)
{
UNUSED(timeout);
UTIL_SEQ_WaitEvt(1U << CFG_EVT_SYSTEM_HCI_CMD_EVT_RESP);
return;
}

I’ve tried to compare example ioc file and mine and can't find something

 

Could, someone, please help me find what I've missed?

This topic has been closed for replies.
OuadiBest answer
ST Technical Moderator
Mar 26, 2025 2:37 PM UTC

Hi,

From the IOC file, I noticed that the traces are not set correctly, so the program get stuck in the DbgTrace func.

When enabling Traces for Zigbee, please enable also the circular buffer as follow :

Ouadi_0-1742999707539.png

After generating the project, make sure to call the func Init_Debug() in MX_APPE_Init() to initialize the UART.

Hope this helps.

Best regards,

Ouadi

3 replies

OuadiBest answer
ST Technical Moderator
Mar 26, 2025 2:37 PM UTC

Hi,

From the IOC file, I noticed that the traces are not set correctly, so the program get stuck in the DbgTrace func.

When enabling Traces for Zigbee, please enable also the circular buffer as follow :

Ouadi_0-1742999707539.png

After generating the project, make sure to call the func Init_Debug() in MX_APPE_Init() to initialize the UART.

Hope this helps.

Best regards,

Ouadi

_Garacio_Author
Associate II
Mar 26, 2025 11:09 PM UTC

Hm...thank you!
It really works!

It's strange, but if I use Init_Debug() inMX_APPE_Init(), I should fix the autogenerated MX_USART1_UART_Init from static to exportable function and move the definition to main.h.

CubeMX generates it as static function thus it can't be used from another file and I should fix it every time I have regenerate the code

ST Technical Moderator
Mar 27, 2025 9:51 AM UTC

Hi,

 MX_USART1_UART_Init is already called in the main and has not to be called in the app_entry.c, We will fix this issue in the upcoming release of CubeMX.

Best regards,

Ouadi