Skip to main content
CBras
Associate II
Mar 19, 2025 1:34 PM UTC
Question

X-NUCLEO-WB05KN1 - Zephyr Problem

Hi,

I have attached a X-NUCLEO-WB05KN1 on top of a NUCLEO-H743ZI2 board and are trying to verify whether it works by flashing the peripheral_hr sample with the shield argument "x_nucleo_wb05kn1_spi". Sadly it does not work (it is stuck in bt_spi_open when trying to receive SPI header from shield)

The shield is flashed such that it uses SPI instead of UART.

I have done the same experiment, placing the shield on top of Nordic Semiconductors' nRF52840 MCU and here it works with the peripheral_hr sample with shield argument.

I have also tried the experiment on a NUCLEO-F401RE and here it also fails.

Any ideas what could be wrong?

This topic has been closed for replies.

4 replies

CBras
CBrasAuthor
Associate II
Mar 24, 2025 6:34 AM UTC

Any updates?

STTwo-32
ST Technical Moderator
Apr 28, 2025 12:48 PM UTC

Hello @CBras 

This behavior has been escalated internally (under internal ticket number 208694). I will get back to you ASAP.

Best Regards.

STTwo-32  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
May 16, 2025 4:01 PM UTC

I'm experiencing the same issue

CBras
CBrasAuthor
Associate II
May 19, 2025 5:08 AM UTC

I was handed a temporary solution almost a month ago but it doesn't seem like the right fix has been provided to upstream zephyr.. I have attached the file.