Skip to main content
CBras
Associate II
Jun 2, 2025 12:28 PM UTC
Question

X-NUCLEO-WB05KN1 Bootloader

Hi,

I'm trying to enter bootloader mode but fails in the process.

Things i have done:

Shield powered with 3.3V

FTDI attached to RXD, TXD, GND

JP1 changed from User Flash -> Bootloader

Measured that PA10 is high at boot

I send 0x7F but doesn't receive anything.

Oscilloscope used to be sure that 0x7F is transmitted

Any suggestions on next steps? 

This topic has been closed for replies.

4 replies

STTwo-32
ST Technical Moderator
Jun 2, 2025 12:50 PM UTC

Hello @CBras 

Could you please try to access bootloader using the STM32CubeProgrammer V2.19.0 and give as the logs (with verbosity level 3). Also, what are the setting that you are using (are you using PA1 as TX and PB0 as RX for USART configured to 8-bit, no parity).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CBras
CBrasAuthor
Associate II
Jun 2, 2025 1:01 PM UTC

I should have mentioned that i already try in STM32CubeProgrammer.

Yes I use PA1 and PB0 which from what I see on schematic for shield is available on the arduino pins.

Serial is set to 8-bit no parity, 9600 bps and 115200 are tried.

I have attached the logs

14:55:35:651 : UR connection mode is defined with the HWrst reset mode
14:55:35:661 : RTS low
14:55:35:661 : DTR low
14:55:35:674 : Serial Port COM5 is successfully opened.
14:55:35:674 : Port configuration: parity = none, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
14:55:35:674 : No Init bits value is : 0
14:55:35:674 : Sending init command:
14:55:35:676 : #byte 0x7F sent successfully to target
14:55:37:677 : Wait ends after 1 loop, dataready = 0, delay = 2000
14:55:37:677 : Timeout error occured while waiting for acknowledgement.
14:55:37:678 : No response from target received
14:55:37:678 : Retrying UART init connection...
14:55:37:680 : #byte 0x7F sent successfully to target
14:55:37:778 : Wait ends after 1 loop, dataready = 0, delay = 100
14:55:37:779 : Timeout error occured while waiting for acknowledgement.
14:55:37:781 : No response from target received
14:55:37:781 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
14:55:37:894 : UART PORT CLOSE

CBras
CBrasAuthor
Associate II
Jun 3, 2025 4:03 AM UTC

@STTwo-32 when I have changed the jumper from User Flash -> Bootloader, it no longer work in my application with SPI so I assume it is in bootloader mode.

STTwo-32
ST Technical Moderator
Jun 30, 2025 3:09 PM UTC

Hello @CBras 

Sorry for my late feedback, to enter UART bootloader mood on the X-NUCLEO-WB05KN1 you have too:

  1. Connect the X-NUCLEO-WB05KN1 to a host board (NUCLEO-U575ZI-Q for example).
  2. Set the jumper JP1 to bootloader mood.
  3. Connect the CN5 RESET pin to a 3V3 source (external not the one from the shield).
  4. Connect the RX and TX pins of the CN7 to the TX and RX of your FTDI respectively.
  5. Connect using those options on the STM32CXubeProgrammer (V2.19.0):

     
     

     

  6. It should work fine:                                                                                                      STTwo32_7-1751296161658.png

     

    Best Regards.

     

    STTwo-32 
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.