Skip to main content
Associate
Oct 22, 2025 12:27 PM UTC
Question

Wrong SystemCoreClock value after SystemCoreClockUpdate (HSE with HSEPRE=2)

Hello,

I use a STM32WLE5JCI6 MCU. Sometimes I need a good clock precision so I switch to HSE as SYSCLK, with a 32MHz quartz. I use 4MHz as HCLK, and I chose to set HSEPRE=2 and HPRE=4. When I call SystemCoreClockUpdate() function the SystemCoreClock value is 8MHz, because HSEPRE value is not considered. Is it a bug or this is the expected value, for any reason I missed? The function HAL_RCC_GetSysClockFreq() uses LL_RCC_HSE_IsEnabledDiv2 to return the expected value, so the SystemCoreClock value is 4MHz if I configure the HSE as sysclock at startup.

Thanks,

Sylvain

 

My code:

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSEDiv = RCC_HSE_DIV2;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK3|RCC_CLOCKTYPE_HCLK
 |RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1
 |RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV8;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK3Divider = RCC_SYSCLK_DIV8;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable the HSE Prescaler
 */
 __HAL_RCC_HSE_DIV2_ENABLE();
 HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_SYSCLK, RCC_MCODIV_1);
}

and:

int main(void)
{
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* Configure the system clock */
 SystemClock_Config();

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART1_UART_Init();

 printf("Test HSE. %s - %s\n\r", __DATE__, __TIME__);
 printf("SystemCoreClock = %lu\r\n", SystemCoreClock);
 SystemCoreClockUpdate();
 printf("SystemCoreClock = %lu\r\n", SystemCoreClock);

 

Result:

Test HSE. Oct 22 2025 - 13:59:06
SystemCoreClock = 2000000
SystemCoreClock = 4000000

 

 

This topic has been closed for replies.

2 replies

TDK
Oct 22, 2025 1:29 PM UTC

Sure looks like a bug. Most chip don't have an HSEPRE field so it probably got missed.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Oct 22, 2025 2:06 PM UTC

Thanks for your answer. Is it safe to do this as a workaround?

 

/* Update the SystemCoreClock global variable */

SystemCoreClock = HAL_RCC_GetHCLKFreq();