Skip to main content
Visitor II
Jun 21, 2025 5:43 AM UTC
Solved

Write to flash while running from the same flash.

I am implementing a dual-bank-like firmware architecture on the STM32WLE5CCU6 microcontroller, which does not natively support true dual-bank flash. In this setup, I need to write data to a region of the internal Flash memory that is part of the same memory space from which the code is currently executing. I would like to understand how Flash write operations can be safely performed in such a scenario—specifically, how to write to a different section of the same Flash memory while code execution continues from another region within that same Flash.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 4, 2025 9:59 AM UTC

Hello @jackiee 

While writing/erasing into Flash bank then there is not possible to perform any else operation from the same bank (read, execute). But read/execute operation is possible from another bank (if this bank is not under write/erase operation).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 4, 2025 9:59 AM UTC

Hello @jackiee 

While writing/erasing into Flash bank then there is not possible to perform any else operation from the same bank (read, execute). But read/execute operation is possible from another bank (if this bank is not under write/erase operation).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.