Skip to main content
j.villar
Associate
Feb 13, 2023 11:39 AM UTC
Solved

Why does BLE stop advertising when STM32WB enters low power mode (STOP2)?

Hello,

 

I am trying to configure a custom board with STM32WB5MMG in STOP2 low power mode. For that, the program calls the PWR_ExitStopMode() function when a timer reaches 10 seconds and exits when EXTI0 interrupts by calling PWR_ExitStopMode().

 

The MCU goes into and exits from STOP2 mode correctly, but I need the board remain connectable even when the MCU is in low power mode; however, BLE stops advertising when the board is in STOP2 mode.

 

If the connection has been established before the board goes into stop mode, then BLE works fine until a disconnection occurs, then I have the same problem.

 

I also tried using sleep mode and got the same results.

 

Code:

__weak void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

{

if(GPIO_Pin == BTN_Pin)

{

PWR_ExitSleepMode();

//SystemClock_Config();

HAL_TIM_Base_Start_IT(&htim2);

printf("WAKE UP FROM EXTI\r\n");

}

}

 

in main:

 

if(timer_1s>=10)

{

PWR_EnterStopMode();

printf("GOING INTO STOP2 MODE\r\n");

}

 

What I'm missing?

Thanks in advance!

This topic has been closed for replies.
Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Feb 17, 2023 11:02 AM UTC

Hello,

See my response in this thread:

Why does BLE become not discoverable when STM32WB goes into low power mode?

Best Regards

2 replies

Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Feb 17, 2023 11:02 AM UTC

Hello,

See my response in this thread:

Why does BLE become not discoverable when STM32WB goes into low power mode?

Best Regards

j.villar
j.villarAuthor
Associate
Feb 20, 2023 6:18 AM UTC

Hi,

Sorry I've duplicate the question unintentionally!