Skip to main content
DGert.1
Associate
Apr 27, 2023 11:10 PM UTC
Solved

Why does B-L072Z-LRWAN1 optionally allow 32MHz clock to PHY_OSC_IN?

According to the user manual (st (dot) com/resource/en/user_manual/um2115-discovery-kit-for-lorawan-sigfox-and-lpwan-protocols-with-stm32l0-stmicroelectronics.pdf), you can optionally close SB13 to get a 32MHz clock signal to the MCU instead of attaching your own external clock. However, when selecting the clock configuration for the STM32L072CZYx the HSE crystal freq is only allowed up to 25MHz and I see similar information in the datasheet for STM32L072xZ (st (dot) com/resource/en/datasheet/stm32l072cz.pdf).

Maybe I am just misunderstanding but it sure seems like the intent is for the TXCO to be routed to the PHY_OSC_IN pin on the MCU in some applications, but the MCU is only rated for 25MHz

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 27, 2023 11:58 PM UTC

fHSE_ext is 32 MHz

25 MHz is for the oscillator (OSC_IN / OSC_OUT)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 27, 2023 11:58 PM UTC

fHSE_ext is 32 MHz

25 MHz is for the oscillator (OSC_IN / OSC_OUT)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DGert.1
DGert.1Author
Associate
Apr 28, 2023 12:13 AM UTC

Thank you so much! That was it, just needed to read the datasheet more carefully