Skip to main content
Salvatore1
Associate
December 2, 2020
Question

Why device using I-Cube-LRWAN software send random data when uplink_counter reach 65535 sent ? Is there any way to modify it ?

Hello Everyone,

I'm working with the I-Cube-LRWAN software for LoRa communication in class A device.

The device sends data every Tx_Dutycyle period but I have an issue with the software.

When using the stack connected to Network such as TTN, I notice the uplink counter reach a threshold after 65535 sent.

Then, It sends some random data and don't follow the data in the Send function.

Where can i change or renew the tx_counter to avoid this issue ? I don't know where i can found this. Furthermore, in "LoraMac.h" i can see in the following structure "typedef struct sMcpsConfirm" the following stuff :

  /*!

   * The uplink counter value related to the frame

   */

  uint32_t UpLinkCounter;

If it's a uint32_t, why there is a problem after 65535 value sent ?  

here your can see an example of data sent with the counter at 65535 and the next one with a totally other payload and the counter at 0.

Then, all the following data are randomised by the software.

{

   "dev_id": "xxxx"

   "hardware_serial": "xxxxx",

   "port": 2,

   "counter": 65535,

   "payload_raw": "CWcA/gpoTQsCH1QMAiTSDQIfCg7/AAAAD/8AAl4QfQAADxFn6D4SAgDb",

   "metadata": {

       "time": "2020-11-27T02:26:44.743301225Z",

      "frequency": 868.3,

      "modulation": "LORA",

       "data_rate": "SF10BW125", ...

{

   "dev_id": "xxxx",

   "hardware_serial": "xxxxx",

   "port": 2,

   "counter": 0,

   "payload_raw": "nNV0JDL2qpzGxKJwFCx42vfkUzNC/hb3KfmjaI9ZQg/K6Q6ahIv5CgKF",

   "metadata": {

       "time": "2020-11-27T02:31:44.878152859Z",

       "frequency": 868.3,

       "modulation": "LORA",

       "data_rate": "SF10BW125",...

Hope you will help me.

Many thanks !

Salvatore

#I-CUBE-LRWAN​  #LoRa​ 

This topic has been closed for replies.