Skip to main content
Selim Sagir
Associate III
August 27, 2019
Question

Which files require for only LoRa communication in the i-cube-lrwan library?

  • August 27, 2019
  • 1 reply
  • 482 views

Hello,

I want to use only LoRa communication between to devices. Which files i need for this in the i-the cube-lrwan library. I going to add this files to CubeMX project.

Regards.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
August 27, 2019

The code is spread across multiple files, at the end of the day you might just need to port some SPI code, the SX127x radio hw code and some interrupt handlers.

The Ping-Pong code is a minimal build for the LRWAN library code, without the LoRaWAN support code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..