Skip to main content
MK..1
Associate III
Oct 1, 2022 10:36 AM UTC
Question

which example project/ video tutorial for sending data to a stm32wb55rg nucleo via python & BLE

Hi

I need to send (and possbly receive) data via BLE and python to a Stm32wb55RG Nucleo board. THere are so many examples. Which one should I Take or which one is best suited for me as a starting point?

I am trying not to watch 100s of videos. Or Do I need to watch them all? ;)

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Oct 3, 2022 1:32 AM UTC

Perhaps get a file manager, or grep the sources to narrow things down a little

Or team up with similarly motivated members

https://community.st.com/s/question/0D53W00001qJ8YKSA0/stm32wb-nucleo-please-share-an-example-to-send-data-from-stm-to-the-computer-via-ble

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Employee
Oct 13, 2022 11:08 AM UTC

Hello @MK..1​ and welcome to the community 

You can start with this link:

public/stm32python/bluetooth-low-energy/nucleo-wb55 · master · STM32 Python / assets · GitLab

I have to mention that some concerned scripts are still under development, thus, if u have any problem, you can mention it here.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.