Skip to main content
Associate III
Dec 22, 2025 3:15 PM UTC
Question

Where to start developing a Firmware for a On/off Light with philips hue

Hi there,

i am planning to create a "smart light" (on/off) which is compatible with philips hue with a stm32wb55RG (nucleo).

I have digged a bit into the numerous examples for zigbee applications and also tried some of them, basically the on/off examples with two boards. They worked and all is fine.

Now i am about to gather informations what would be the best start of getting this into my Hue Bridge.

Currently my Bride does not see those end devices from the example, so i can not add it there.

Does anyone has some kind of Tip or Setup which you can share which is aiming to work with Hue?

 

Thank you