Skip to main content
ledi001
Associate III
Oct 17, 2024 1:23 PM UTC
Solved

Where can i find the OTA-Bootloader for STM32WBA55

Hi,

where can i find the OTA-Bootloader for STM32WBA55?

For STM32WB it is located in the regarding FW-Package in Folder "BLE_Ota", but in the FW-Package of STM32WBA i can't find it there.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Oct 17, 2024 1:57 PM UTC

Hello @ledi001 

For the OTA on the STM32WBA, there is no binary file such as the "BLE_OTA" on the STM32WB. The only available firmware examples for OTA on the STM32WBA are BLE_HeartRate_ota and  BLE_p2pServer_ota.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Oct 17, 2024 1:57 PM UTC

Hello @ledi001 

For the OTA on the STM32WBA, there is no binary file such as the "BLE_OTA" on the STM32WB. The only available firmware examples for OTA on the STM32WBA are BLE_HeartRate_ota and  BLE_p2pServer_ota.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ledi001
ledi001Author
Associate III
Oct 26, 2024 8:53 AM UTC

Hello @STTwo-32 ,

thanks for information.

But when i check the linker script files, i see these Memory Definitions:

BLE_p2pServer_ota

/* Memories definition */
MEMORY
{
 RAM (rw) : ORIGIN = 0x20000020, LENGTH = (128K - 0x20)

 NVM (r) : ORIGIN = 0x080FC000, LENGTH = 16K
 DATA (r) : ORIGIN = 0x080FA000, LENGTH = 8K
 FLASH (rx) : ORIGIN = 0x08006000, LENGTH = 488K
}

 

BLE_ApplicationInstallManager

/* Memories definition */
MEMORY
{
 RAM (rw) : ORIGIN = 0x20000010, LENGTH = (0x10000 - 0x10)

 FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 0x6000
}

In this case, so if the OTA bootloader is included here for BLE_p2pServer_ota, shouldn't the area for the flash also start at 0x0800 0000? 

 

STTwo-32
ST Technical Moderator
Oct 26, 2024 10:46 AM UTC

Hello @ledi001 

This is a new question. Could you please close this topic by selecting the answer of your original question as best answer. Then, create a post for your New question with more details if possible.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
Oct 24, 2024 9:55 AM UTC

Hi, 
You can find more information on how OTA works on WBA here :
STM32WBA Bluetooth® LE – Firmware update over the air - stm32mcu

BR, Joé