Skip to main content
HCohe.1
Associate III
Mar 29, 2022 4:27 PM UTC
Solved

Where can I find an up-to-date version of BLE_HeartRate_ota for STM32WB?

The readme.txt file for BLE_HeartRate_ota contains the following:

@note This application is not supported by CubeMx but has been copied from the project BLE_HeartRate generated
 by CubeMx with some modifications in order to be able to download it with the BLE_Ota application.
	 The steps to be done to move from the BLE_HeartRate application to the BLE_HeartRate_ota application are :
	 - Copy the full folder BLE_HeartRate
	 - Replace the linker file stm32wb55xx_flash_cm4.icf by stm32wb55xx_flash_cm4_ota.icf ( this adds the placement
	 of the two sections TAG_OTA_START and TAG_OTA_END ).
	 - Remove the update of SCB->VTOR in the file system_stm32wbxx.c ( The VTOR is already set by the BLE_Ota application
	 and shall not be changed to a different value)
 - set BLE_CFG_OTA_REBOOT_CHAR to 1 in ble_conf.h

However, comparing the two source directories I see many more differences and find it difficult to identify and merge all of the required modifications. BLE_HeartRate_ota does not appear to have all the newer features and bug fixes applied. Will we see a updated version in the next release?

This topic has been closed for replies.
Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 30, 2022 4:08 PM UTC

Hello,

Indeed BLE_HeartRate and BLE_HeartRate_ota projects aren't aligned, it will be updated in the next release v1.14.0. In order to have only the differences describe in your screenshot between the two projects.

Best Regards

1 reply

Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 30, 2022 4:08 PM UTC

Hello,

Indeed BLE_HeartRate and BLE_HeartRate_ota projects aren't aligned, it will be updated in the next release v1.14.0. In order to have only the differences describe in your screenshot between the two projects.

Best Regards