Where can I download the version of the wireless stack v16.12.0.27
The previous developer developed a device based on STM32wb55. We were produced an anower such device and flashed with the same firmware and wireless stack version 1.14.0. The new device communicates with the our test software, but loses communication at random intervals, although the first board does not have this problem. The hardware part is checked and completely identical, the software too. Obviously the problem is in the stack version. Reading the stack version of the first board gives the following result - Stack Version - v16.12.0.27, FUS version v0.0.0.0. I think the embedded software work properly only with this particular stack version, but i don't now what Cube Packgage verion contains it. e?Where i am need to looking for? Or, may be here is anower problem, which i don't see?