Just used the example application "LoRaWan_End_Node" with the Nucleo-WLWL55JC board.
This example send every 10seconds data to a gateway which is received in the TheThingsNetwork environment.
Default is "LoRaWan_End_Node" disabled, when "USE_FULL_ASSERT" is enabled the applciation starts working and data is received, but after first time or after some rounds (within some minutes) the application keeps trying to send data, but data is not received at the server or the attempts are stopped. There is not assert or error in debugger.
When "USE_FULL_ASSERT" is disabled again, the data is received okay at server endless time.
In the stm32wlxx_hal_rtc.c source file some additional checks are done when USE_FULL_ASSERT is enabled. Can this be the problem?
In attachment some logging.