Skip to main content
HAgar.1
Associate II
Jul 10, 2021 5:54 PM UTC
Question

What values of pull-up resistors should be used for the BOOT0 and BOOT1 pins in the STM32WB30CE MCU? They are not mentioned in the datasheet for the MCU.

..

This topic has been closed for replies.

10 replies

TDK
Jul 10, 2021 10:53 PM UTC

10 kOhm is typical, but the pin is floating internally so values far higher than this will work as well without drawing additional current.

"If you feel a post has answered your question, please click ""Accept as Solution""."
HAgar.1
HAgar.1Author
Associate II
Jul 11, 2021 3:27 PM UTC

What values would you suggest?

TDK
Jul 11, 2021 3:32 PM UTC

10 kOhm.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Uwe Bonnes
Chief
Jul 11, 2021 11:35 AM UTC

If working in a high temperature environment, leckage current increase substantial and the 10 kOhm might need reconsideration.

HAgar.1
HAgar.1Author
Associate II
Jul 11, 2021 3:27 PM UTC

How high are we talking about?

Uwe Bonnes
Chief
Jul 11, 2021 3:28 PM UTC

To be one the safe side, look at the max. values in the appropriate datasheet.

HAgar.1
HAgar.1Author
Associate II
Jul 11, 2021 7:30 PM UTC

That's the issue, they are not mentioned in the datasheet for this MCU