Skip to main content
KOr.1
Associate
Aug 10, 2022 9:22 PM UTC
Question

What should be the correct SBRV value after flashing stm32wb5x_BLE_Stack_full_fw at 0x080CE000 using FUS version 1.2.0 ? MCU is STM32WB5xxG(1M)

..

This topic has been closed for replies.

2 replies

Remy ISSALYS
ST Technical Moderator
Aug 17, 2022 9:30 AM UTC

Hello,

According to the AN5185:

  • If SBRV Option Bytes value is 0x3D800 (for FUS V0.5.3) or 0x3D000 (for FUS V1.x.z) then FUS must be running
  • If SBRV Option Bytes value is different from 0x3D800 (for FUS V0.5.3) and from 0x3D000 (for FUS V1.x.z) then FUS is not running

Best Regards

Remi QUINTIN
ST Technical Moderator
Aug 26, 2022 10:46 AM UTC

And in that case the SBRRV option byte should be pointing at the start of the wireless stack, which, in case of a successful installation at 0x080CE000, should be 0x33800