Skip to main content
VVakh.1
Associate II
Feb 8, 2022 9:29 PM UTC
Solved

What is the soldering profile for the STM32WB35CCU6A MCU?

The operating temperature range for the above MCU is -40 to 85 deg C (105 deg C junction). Does it mean that the maximum temperature for soldering is 105 deg C, or does it just mean that the MCU will shut down at 105 deg C? I would appreciate it if you refer to any official application note.

This topic has been closed for replies.
TDK
TDKBest answer
Feb 9, 2022 2:35 AM UTC

85C (105C junction) is the max operating temperature. Junction temperature is what actually matters here. Beyond that range the behavior is no longer guaranteed.

Soldering will need to be quite a bit hotter.

https://www.st.com/resource/en/application_note/an2639-soldering-recommendations-and-package-information-for-leadfree-ecopack-mcus-and-mpus-stmicroelectronics.pdf

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Feb 9, 2022 2:35 AM UTC

85C (105C junction) is the max operating temperature. Junction temperature is what actually matters here. Beyond that range the behavior is no longer guaranteed.

Soldering will need to be quite a bit hotter.

https://www.st.com/resource/en/application_note/an2639-soldering-recommendations-and-package-information-for-leadfree-ecopack-mcus-and-mpus-stmicroelectronics.pdf

"If you feel a post has answered your question, please click ""Accept as Solution""."
VVakh.1
VVakh.1Author
Associate II
Feb 9, 2022 2:51 PM UTC

Thank you