Skip to main content
kiwironnie
Associate III
Jul 26, 2020 3:15 AM UTC
Question

What is the least effort process to modify a LRWN expansion example project for the STM32L476 mcu, imported as a file system project into STM32CubeIDE , to instead support an STM32L433 mcu?

Not sure if this is the best place to ask, but essentially I want to modify the LoRaWAN end-node example for STM32L476 using SX1262 transceiver to work with an STM32L433 mcu, initially making use of a Nucleo-L433RC-P board with a transceiver module wired to it, eventually shifting this to a custom board with STM32L433.

Have done something similar before for the STM32L073 processor, although that was more straightforward as that mcu is one of the example ones provided in the STM LoRaWAN code.

This topic has been closed for replies.