Question
What happens when the protocol stack is written to an incorrect address?
Hello.
If I write the protocol stack to an address different from the original address, will the protocol stack work properly? The firmware I wrote is stm32wb5x_Ble_Mac_802_15_4_fw.bin, and I wrote it to 0x080B1000 when it should have been written to 0x080B9000. I don't have the actual firmware so I can't see how it works. I think the protocol stack isn't working properly. Is that correct? Or will it work properly even if I write it to the wrong address?