Skip to main content
GLasw.1
Associate
January 11, 2021
Question

What are the steps to port BLE_MeshLightingProvisioner from P-NUCLEO-WB55.Nucleo to P-NUCLEO-WB55.USBDongle board?

  • January 11, 2021
  • 0 replies
  • 460 views

I have created a board based on STM32WB55CG which is same microcontroller as that is used in P-NUCLEO-WB55.USBDongle.

The problem is, in STM32Cube_FW_WB_V1.10.0 project folder for P-NUCLEO-WB55.USBDongle board, there is no BLE_MeshLightingProvisioner example included.

I have tried to read AN5292 document, but there is nowhere this is mentioned on how to port project from one microcontroller to another.

Also, i have noticed that, the Upper Tester protocols as explained in AN5292 using the provided project BLE_MeshLightingPRFNode are not working either but everything else works; something to do with command not being sent to microcontroller using the VCOM port.

Can anyone help on this?

This topic has been closed for replies.