Question
What are the benefits of using STSAFE security IC to reset a microcontroller?
I am using BL072Z board and the datasheet says:
8.6 Reset sources
The reset signal of the B-L072Z-LRWAN1 Discovery kit is active low and the reset sources is one of the following:
• Reset button B2
• Arduino Uno V3 shield board from CN4
• LoRa®/Sigfox™ module internal reset coming either from STSAFE security IC or
STM32L072CZ (selectable by jumper JP10)
• Embedded ST-LINK/V2-1
But I don't what are the cons if I reset the microcontroller using one of its GPIOs