Skip to main content
TLans.1
Associate
Jul 17, 2024 10:34 AM UTC
Solved

WB55RG/WB15CC and PLC01A1

Is NUCLEO-WB55RG/WB15CC compatible with X-NUCLEO-PLC01A1?

I want to develop a controller that supports BLE and thought of starting with a combination of these two boards. Would be helpful if someone can confirm that these boards are compatible and can be stacked and work together.

Thanks. 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 13, 2024 8:42 AM UTC

Hello @TLans.1 

As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 13, 2024 8:42 AM UTC

Hello @TLans.1 

As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.