Skip to main content
EPekg.1
Visitor II
May 30, 2023 7:50 AM UTC
Question

WB55 board is not appear on bluetooth list

I have a P-NUCLEO-WB55 board and i want to use it to communicate with my phone on ble. Fİrst of all, i decided to try an example to see if its works. I updated fus and then uploaded ble stack like the 11th video of STM32WB Getting Started Series

 After that i decided to try HeartRate example which is shown in 6th video STM32WB Getting Started Series

and i put a breakpoint in APPE_SysUserEvtRx() function. When i debug the code ı observed, program never goes into APPE_SysUserEvtRx(), in fact it stucks after MX_RNG_Init(); function. I made comment this function and i saw this time code stucked on MX_RF_Init(); function. Therefore i believe MX_RTC_Init(); function here causes this stucks. If i make comment the __HAL_RTC_WAKEUPTIMER_ENABLE(hrtc); macro which is in HAL_RTCEx_SetWakeUpTimer_IT() function, it doesnt stuck at init functions but when it come to MX_APPE_Init(); function, it says "Target is not responding, retrying..." then shuts down. Could you please help me?

Best regards..

This topic has been closed for replies.

2 replies

JSanc.7
Associate
Jun 27, 2023 10:47 AM UTC

Hey,

Could you solve this problem? Because I have the same issue and I don't find any solution. 

Thank you.

KKIM.6
Senior
Jul 10, 2023 3:34 PM UTC

In my experience, the BLE doesn't start when debug mod. if you just implant code and check internal massage using USART terminal then you can see a massege like these.11.png