Skip to main content
Mkuma.7
Associate III
Apr 10, 2023 9:47 AM UTC
Question

Via USB interface the -rst using CLI was not working and even in GUI these options were grayed out or not available. I have tried reset=SWrst/HWrst, but it did not work. Is there any way to reset the microcontroller via USB?

Via USB interface the -rst using CLI was not working and even in GUI these options were grayed out or not available. Please refer the below images for reference.Using the WB package - 1.15

Using the STM32Cubeprogrammer - 2.12

Is there any possible way to reset the microcontroller via USB?

This topic has been closed for replies.

6 replies

Aziz BRIGUI
ST Technical Moderator
Apr 19, 2023 11:37 AM UTC

Hello @Mkuma.7​,

Thanks for your feedback,

The reset via USB is only available for MPUs, the screenshot you shared is from the Available commands for STM32 MPU section of the help menu. For MCUs, this instruction is only available via ST-LINK interfaces.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Mkuma.7
Mkuma.7Author
Associate III
Apr 19, 2023 1:15 PM UTC

Hello Aziz BRIGUI,

So you mean there is no way to reset the micro-controller, right?

Mkuma.7
Mkuma.7Author
Associate III
Apr 19, 2023 1:16 PM UTC

I mean via USB

Aziz BRIGUI
ST Technical Moderator
Apr 24, 2023 10:13 AM UTC

Hello @Mkuma.7​,

Yes, as far as I know, there's no way to reset the MCU via USB with STM32CubeProgrammer.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Mkuma.7
Mkuma.7Author
Associate III
Jun 5, 2023 11:34 AM UTC

Hello Aziz,

Is there any way via FUSES to reset the micro-controller?

Mkuma.7
Mkuma.7Author
Associate III
Jun 13, 2023 9:11 AM UTC

@Aziz BRIGUI​ 

Is there any way via FUSES to reset the micro-controller?