Skip to main content
Associate
Aug 25, 2025 8:53 PM UTC
Solved

VDD_TCXO not used at STM2WLE5JCI6

Hi,

We are using the STM32WLE5JCI6.

In our design, the TCXO (HSE) is powered directly by the 3.3 V on-board power supply, and the VDD_TCXO pin is left unconnected.

 

Is this acceptable?

Should we avoid using the Set_TcxoMode command in this case?

Thanks for any help

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 23, 2025 3:44 PM UTC

Hello @Adielfr 

Yes, you can use an external power supply and not the VDD_TCXO pin. This approach is valid as long as the external power supply meets the TCXO's voltage and current requirements. The VDD_TCXO pin is specifically designed to provide power to the TCXO, but it is not mandatory to use it if an external power source is available and suitable. 

For the Set_TcxoMode command, you should not use it in such configuration.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 23, 2025 3:44 PM UTC

Hello @Adielfr 

Yes, you can use an external power supply and not the VDD_TCXO pin. This approach is valid as long as the external power supply meets the TCXO's voltage and current requirements. The VDD_TCXO pin is specifically designed to provide power to the TCXO, but it is not mandatory to use it if an external power source is available and suitable. 

For the Set_TcxoMode command, you should not use it in such configuration.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.