Skip to main content
AElgh
Associate III
Feb 21, 2024 2:00 PM UTC
Question

Using the ST-Link V3E on the STM32WL-Nucleo Board

Hello, 

 

I used the onboard ST-Link Debugger of the STM32F401RE to flash/debug external boards. Can I do the same with the Nucleo-STM32WL55JCx Board(using the MIPI10 Connector)?

 

I checked UM2592, and it only gives directions about using an external debugger(and turning off the on-board one).

 

 

Thank you

Amir

This topic has been closed for replies.

8 replies

STTwo-32
ST Technical Moderator
Apr 15, 2024 1:02 PM UTC

Hello @AElgh 

yes, you can use the Onboard ST-Link Debugger of the STM32F401RE as  an external debug tool to program the on-board STM32WL.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Apr 15, 2024 1:05 PM UTC

I think @AElgh was asking the opposite question?

ie, can the on-board ST-Link of the Nucleo-STM32WL55JCx be used to program/debug an external target?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AElgh
AElghAuthor
Associate III
Apr 15, 2024 1:12 PM UTC

@STTwo-32 exactly as Andrew said, I wanted to use the on board ST-Link of the nucleo STM32WL to debug other boards (using the MIPI10 Connector)