Skip to main content
SBour.9
Associate II
Jun 4, 2019 2:13 PM UTC
Question

Using SX1276MB1LAS with STM32F767ZI.

"The I-CUBE-LRWAN Expansion Package consists of a set of libraries and application examples for STM32L0, STM32L1 and STM32L4 Series microcontrollers acting as end-devices."

Can i use the libraries comming with this package even if i am using a STM32F767ZI and not a STM32Lx?

Simon

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Jun 4, 2019 3:26 PM UTC

You'd have to create an equivalent "shim" layer for the F7, so figure the 10-12 L4 files, to F7 equivalents.

A suggested route is to pivot from L4 NUCLEO-64 to NUCLEO-144, and then pivot from L4 NUCLEO-144 to F767ZI NUCLEO-144, and then to your target hardware.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..