Skip to main content
DS.4
Senior
May 13, 2024 5:21 AM UTC
Solved

Using SHCI_C2_BLE_INIT_OPTIONS_REDUC_GATTDB_NVM to increase bonding list size

Wondering what is the cost of using 

SHCI_C2_BLE_INIT_OPTIONS_REDUC_GATTDB_NVM

over

SHCI_C2_BLE_INIT_OPTIONS_FULL_GATTDB_NVM

?

 

The first one can gets me 33% increase in bonding list size but I could not find what does it prevent me from using?

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 14, 2024 3:29 PM UTC

Hello @DS.4 

The REDUC_GATTDB_NVM can be used in all the cases.

When using the FULL_GATTDB_NVM and SVC_CHANGE_DESC, the GATT database record in NVM is composed as describe in the wiki page by:

  • Per service:
    • 2 bytes for handle
    • 3 bytes if 16-bit UUID or 17 bytes if 128-bit UUID
  • Per characteristic attribute:
    • 2 bytes for handle
    • 3 bytes if 16-bit UUID or 17 bytes if 128-bit UUID
    • 2 bytes for CCCD value (only if the attribute is a CCCD)

When using the REDUC_GATTDB_NVM and SVC_CHANGE_DESC, the GATT database record in NVM is composed by:

  • Per characteristic attribute:
    • 3 bytes for CCCD value (only if the attribute is a CCCD)
      + 16 bytes (The Data Base hash stores a 128 bits value calculated from the Data Base structure. Any change in the Data Base structure results in a different hash value.)

When a connection is established with a previously bonded device, the GATT database is compared with the GATT database saved in NVM. If there is a difference between the databases, a service change indication will be sent to the peer device. The contents of the indication will depend of FULL_GATTDB_NVM and REDUC_GATTDB_NVM flags:

- When using FULL_GATTDB_NVM, you know where the change is located, the service change indication will contain the specific handle of the service/characteristic where there is the modification.
- When using REDUC_GATTDB_NVM, since the data stored in NVM is a hash, it is not possible to know where is located the change, the service change indication will indicate a change of all the database.

 

More details are available on this WiKi.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 14, 2024 3:29 PM UTC

Hello @DS.4 

The REDUC_GATTDB_NVM can be used in all the cases.

When using the FULL_GATTDB_NVM and SVC_CHANGE_DESC, the GATT database record in NVM is composed as describe in the wiki page by:

  • Per service:
    • 2 bytes for handle
    • 3 bytes if 16-bit UUID or 17 bytes if 128-bit UUID
  • Per characteristic attribute:
    • 2 bytes for handle
    • 3 bytes if 16-bit UUID or 17 bytes if 128-bit UUID
    • 2 bytes for CCCD value (only if the attribute is a CCCD)

When using the REDUC_GATTDB_NVM and SVC_CHANGE_DESC, the GATT database record in NVM is composed by:

  • Per characteristic attribute:
    • 3 bytes for CCCD value (only if the attribute is a CCCD)
      + 16 bytes (The Data Base hash stores a 128 bits value calculated from the Data Base structure. Any change in the Data Base structure results in a different hash value.)

When a connection is established with a previously bonded device, the GATT database is compared with the GATT database saved in NVM. If there is a difference between the databases, a service change indication will be sent to the peer device. The contents of the indication will depend of FULL_GATTDB_NVM and REDUC_GATTDB_NVM flags:

- When using FULL_GATTDB_NVM, you know where the change is located, the service change indication will contain the specific handle of the service/characteristic where there is the modification.
- When using REDUC_GATTDB_NVM, since the data stored in NVM is a hash, it is not possible to know where is located the change, the service change indication will indicate a change of all the database.

 

More details are available on this WiKi.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DS.4
DS.4Author
Senior
May 15, 2024 10:27 AM UTC

"When using FULL_GATTDB_NVM, you know where the change is located, the service change indication will contain the specific handle of the service/characteristic where there is the modification.
- When using REDUC_GATTDB_NVM, since the data stored in NVM is a hash, it is not possible to know where is located the change, the service change indication will indicate a change of all the database."

Perfect thanks!