Question
Using MB1389D Nucleo64 with STM32WL on top of Arduino board
Hello there,
I've sucesssfully built the app AT_SLAVE app and downloaded it to my the board.
When connected trough USB everything works fine.
I've the enable USART1 to be able to communicate with the STM32 via D0/D1 of the arduino connector.
I have no communication.
On the arduino board D0 is RX and D1 is TX, but on the Nucleo PB7/PA3(D0) says it is also RX and PB6/PA2 TX (checked trough MX tool).
Any help would be greatly appreciated
Regards
Laurent