Skip to main content
Senior
Jul 26, 2023 11:41 AM UTC
Solved

Using BALFLB-WL-08D3 with STM32WL54CC at 433MHz

Hello,

i need to know if you recommend to use the BALFLB-WL-08D3 at 433MHz

I design my PCB with the STM32WL54CC, and it will operate between 433MHz and 435MHz. i want to know if the BALFLB-WL-08D3 is suitable for my application or if is better to design RF line with passive components.

Thank you,

Sincerely.

This topic has been closed for replies.
IIRHO.1
IIRHO.1Best answer
ST Employee
Jul 26, 2023 3:31 PM UTC

Hello @malarab and welcome to ST Community.

BALFLB-WL-08D3 has a frequency range between 470 and 510MHz. That's why the BALFLB-WL-08D3 is not suitable for your application.

When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster.

Issam

0 Kudos
 
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

IIRHO.1
IIRHO.1Best answer
ST Employee
Jul 26, 2023 3:31 PM UTC

Hello @malarab and welcome to ST Community.

BALFLB-WL-08D3 has a frequency range between 470 and 510MHz. That's why the BALFLB-WL-08D3 is not suitable for your application.

When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster.

Issam

0 Kudos
 
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.