Skip to main content
SCeyl.2
Visitor II
Apr 17, 2023 1:36 PM UTC
Question

Using a nucleo board as programmer

How can i program stm32wle5ccu6 with st-link which is on the nucleo stm32g474ret6 or is it possible?

This topic has been closed for replies.

1 reply

Simon V.
ST Employee
Apr 17, 2023 1:51 PM UTC

Hello,

Sure it is possible, we must remove the solder bridge going from nucleo stlink to imbedded STM32G4 and verify that the target board is also supplied at 3.3V as the nucleo G474 is.

Regards,

Simon

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.