Skip to main content
MLöfg.1
Visitor II
Nov 2, 2022 2:33 PM UTC
Question

Using a MCU with 12-bit ADC to collect data from 24-bit sensor?

I want to use a STM32WB55CG with a 12-bit ACD to collect sensor data from ADS1292R (24-bit ECG sensor) and MAX86150 (19-bit PPG sensor).

Short question: Is this possible?

If so: Any suggestions on how to do so? Do need some external component?

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
Nov 2, 2022 3:14 PM UTC

Yes, that should be possible.The two devices are connected via SPI and I2C respectively, which should not require any additional devices. However, TI sometimes has its own ideas about the format of the SPI transmission.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Piranha
Principal III
Nov 2, 2022 4:21 PM UTC

MCU's ADC has nothing to do with those other devices, with which you communicate through SPI, I2C or other digital connections.

Tesla DeLorean
Guru
Nov 2, 2022 4:38 PM UTC

>> Any suggestions on how to do so? Do need some external component?

If the formats don't conform to the function/expectations of the on-board peripherals, you can presumably use the GPIO's to emulate interactions at some lower bandwidth.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..