Skip to main content
NRedd.2
Associate III
August 12, 2024
Solved

USBX Dual Composite CDC ACM not working

  • August 12, 2024
  • 3 replies
  • 2155 views

Hello all,

 

I am trying to add two virtual COM ports on STM32WB5MMHGx device. The initial code is based out of STM32Cube example: Ux_Device_CDC_ACM.

I initially added this piece of code to register the class.

 

 

 

 cdc_acm_parameter2.ux_slave_class_cdc_acm_instance_activate = USBD_CDC_ACM_Activate2;
 cdc_acm_parameter2.ux_slave_class_cdc_acm_instance_deactivate = USBD_CDC_ACM_Deactivate2;
 cdc_acm_parameter2.ux_slave_class_cdc_acm_parameter_change = USBD_CDC_ACM_ParameterChange2;

 uint32_t code;
 if ( code = ux_device_stack_class_register("ACM2",
 ux_device_class_cdc_acm_entry,
 cdc_acm_configuration_number,
 cdc_acm_interface_number,
 &cdc_acm_parameter2) != UX_SUCCESS )
 {
 UNUSED(code);
 /* USER CODE BEGIN USBX_DEVICE_CDC_ACM_REGISTER_ERORR */
 return UX_ERROR;
 /* USER CODE END USBX_DEVICE_CDC_ACM_REGISTER_ERORR */
 }

 

 

 

 Memory pool and USB stack sizes were increased so that this registration process succeds.

That did not show up as two ACM devices on linux. After digging around, I found that there is a bug in the ux_device_descriptors.c. 

 

This piece of code is needed to enumerate and add two classes.

 

 

 

uint8_t UserClassInstance[USBD_MAX_CLASS_INTERFACES] = {
 CLASS_TYPE_CDC_ACM,
 CLASS_TYPE_CDC_ACM
};

 

 

 

 But that does not add proper descriptors and endpoint addresses. I solved this by comparing with NXP device descriptors. 

 

The changes made to get two devices listed as ttyACM1 and ttyACM2 are:

 

 

 

uint8_t USBD_FrameWork_AddToConfDesc(USBD_DevClassHandleTypeDef *pdev, uint8_t Speed,
 uint8_t *pCmpstConfDesc)
{
.
.
.

 switch (pdev->tclasslist[pdev->classId].ClassType)
 {

#if USBD_CDC_ACM_CLASS_ACTIVATED == 1

 case CLASS_TYPE_CDC_ACM:

 /* Find the first available interface slot and Assign number of interfaces */
 interface = USBD_FrameWork_FindFreeIFNbr(pdev);
 pdev->tclasslist[pdev->classId].InterfaceType = interface; //! Assign missing interface number.
 pdev->tclasslist[pdev->classId].NumIf = 2U;
}

 

 

 

 And the address was incremented by InterfaceType.

 

 

 

 

static void USBD_FrameWork_AssignEp(USBD_DevClassHandleTypeDef *pdev,
 uint8_t Add, uint8_t Type, uint32_t Sze)
{
 uint32_t idx = 0U;

 /* Find the first available endpoint slot */
 while (((idx < (pdev->tclasslist[pdev->classId]).NumEps) && \
 ((pdev->tclasslist[pdev->classId].Eps[idx].is_used) != 0U)))
 {
 /* Increment the index */
 idx++;
 }

 /* Configure the endpoint */
 uint8_t address = Add + pdev->tclasslist[pdev->classId].InterfaceType;
 pdev->tclasslist[pdev->classId].Eps[idx].add = address;
 pdev->tclasslist[pdev->classId].Eps[idx].type = Type;
 pdev->tclasslist[pdev->classId].Eps[idx].size = (uint16_t) Sze;
 pdev->tclasslist[pdev->classId].Eps[idx].is_used = 1U;
}

 

 

 

This fixed the issue. Now I see two VCOMs.

 

 

[ +0.300216] usb 1-4.3.4: new full-speed USB device number 89 using xhci_hcd
[ +0.190420] usb 1-4.3.4: New USB device found, idVendor=0483, idProduct=5740, bcdDevice= 2.00
[ +0.000005] usb 1-4.3.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000002] usb 1-4.3.4: Product: STM32 Virtual ComPort
[ +0.000002] usb 1-4.3.4: Manufacturer: STMicroelectronics
[ +0.000001] usb 1-4.3.4: SerialNumber: CDC_ACM001
[ +0.016028] cdc_acm 1-4.3.4:1.0: ttyACM1: USB ACM device
[ +0.000428] cdc_acm 1-4.3.4:1.2: ttyACM2: USB ACM device

 

 

 

Also, I added the addresses to the init function:

 

 

 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x00 , PCD_SNG_BUF, 0x14);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x80 , PCD_SNG_BUF, 0x54);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x81, PCD_SNG_BUF, 0x94);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x01, PCD_SNG_BUF, 0xD4);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x82, PCD_SNG_BUF, 0x114);

 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x02 , PCD_SNG_BUF, 0x154);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x82 , PCD_SNG_BUF, 0x194);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x83, PCD_SNG_BUF, 0x1D4);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x03, PCD_SNG_BUF, 0x214);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x84, PCD_SNG_BUF, 0x254);

 

 

I am not sure if the above is configuration is correct. I have simply followed the pattern.

 

Issue: 

When two CDC ACM classes are added to device_framework_full_speed, I get gibberish on the COM port.

Simply removing CLASS_TYPE_CDC_ACM from UserClassInstance makes a single COM port and UART work as per the initial example.

 

I am definitely missing something. Can anyone help me out? 

Here is a link to the complete project on GitHub. 

 

This topic has been closed for replies.
Best answer by NRedd.2

Hi @FBL ,

 

Thank you for the response!

 

Here I have both the ACM's working with USBx stack.

[Sep 9 14:33] usb 1-4.2.1.1: USB disconnect, device number 16
[ +0.185932] usb 1-4.2.1.1: new full-speed USB device number 17 using xhci_hcd
[ +0.090350] usb 1-4.2.1.1: New USB device found, idVendor=0483, idProduct=5710, bcdDevice= 2.00
[ +0.000006] usb 1-4.2.1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000002] usb 1-4.2.1.1: Product: STM32 USB Device
[ +0.000002] usb 1-4.2.1.1: Manufacturer: STMicroelectronics
[ +0.000002] usb 1-4.2.1.1: SerialNumber: 000000000001
[ +5.275823] cdc_acm 1-4.2.1.1:1.0: ttyACM0: USB ACM device
[ +0.717204] cdc_acm 1-4.2.1.1:1.2: ttyACM2: USB ACM device

 

3 replies

NRedd.2
NRedd.2Author
Associate III
August 13, 2024
Bus 001 Device 032: ID 0483:5740 STMicroelectronics Virtual COM Port
Device Descriptor:
 bLength 18
 bDescriptorType 1
 bcdUSB 2.00
 bDeviceClass 239 Miscellaneous Device
 bDeviceSubClass 2 [unknown]
 bDeviceProtocol 1 Interface Association
 bMaxPacketSize0 64
 idVendor 0x0483 STMicroelectronics
 idProduct 0x5740 Virtual COM Port
 bcdDevice 2.00
 iManufacturer 1 STMicroelectronics
 iProduct 2 STM32 Virtual ComPort
 iSerial 3 CDC_ACM001
 bNumConfigurations 1
 Configuration Descriptor:
 bLength 9
 bDescriptorType 2
 wTotalLength 0x008d
 bNumInterfaces 4
 bConfigurationValue 1
 iConfiguration 0 
 bmAttributes 0xc0
 Self Powered
 MaxPower 50mA
 Interface Association:
 bLength 8
 bDescriptorType 11
 bFirstInterface 0
 bInterfaceCount 2
 bFunctionClass 2 Communications
 bFunctionSubClass 2 Abstract (modem)
 bFunctionProtocol 1 AT-commands (v.25ter)
 iFunction 0 
 Interface Descriptor:
 bLength 9
 bDescriptorType 4
 bInterfaceNumber 0
 bAlternateSetting 0
 bNumEndpoints 1
 bInterfaceClass 2 Communications
 bInterfaceSubClass 2 Abstract (modem)
 bInterfaceProtocol 1 AT-commands (v.25ter)
 iInterface 0 
 CDC Header:
 bcdCDC 1.10
 CDC Call Management:
 bmCapabilities 0x00
 bDataInterface 1
 CDC ACM:
 bmCapabilities 0x02
 line coding and serial state
 CDC Union:
 bMasterInterface 0
 bSlaveInterface 1 
 Endpoint Descriptor:
 bLength 7
 bDescriptorType 5
 bEndpointAddress 0x82 EP 2 IN
 bmAttributes 3
 Transfer Type Interrupt
 Synch Type None
 Usage Type Data
 wMaxPacketSize 0x0008 1x 8 bytes
 bInterval 5
 Interface Descriptor:
 bLength 9
 bDescriptorType 4
 bInterfaceNumber 1
 bAlternateSetting 0
 bNumEndpoints 2
 bInterfaceClass 10 CDC Data
 bInterfaceSubClass 0 [unknown]
 bInterfaceProtocol 0 
 iInterface 0 
 Endpoint Descriptor:
 bLength 7
 bDescriptorType 5
 bEndpointAddress 0x01 EP 1 OUT
 bmAttributes 2
 Transfer Type Bulk
 Synch Type None
 Usage Type Data
 wMaxPacketSize 0x0040 1x 64 bytes
 bInterval 0
 Endpoint Descriptor:
 bLength 7
 bDescriptorType 5
 bEndpointAddress 0x81 EP 1 IN
 bmAttributes 2
 Transfer Type Bulk
 Synch Type None
 Usage Type Data
 wMaxPacketSize 0x0040 1x 64 bytes
 bInterval 0
 Interface Association:
 bLength 8
 bDescriptorType 11
 bFirstInterface 2
 bInterfaceCount 2
 bFunctionClass 2 Communications
 bFunctionSubClass 2 Abstract (modem)
 bFunctionProtocol 1 AT-commands (v.25ter)
 iFunction 0 
 Interface Descriptor:
 bLength 9
 bDescriptorType 4
 bInterfaceNumber 2
 bAlternateSetting 0
 bNumEndpoints 1
 bInterfaceClass 2 Communications
 bInterfaceSubClass 2 Abstract (modem)
 bInterfaceProtocol 1 AT-commands (v.25ter)
 iInterface 0 
 CDC Header:
 bcdCDC 1.10
 CDC Call Management:
 bmCapabilities 0x00
 bDataInterface 3
 CDC ACM:
 bmCapabilities 0x02
 line coding and serial state
 CDC Union:
 bMasterInterface 2
 bSlaveInterface 3 
 Endpoint Descriptor:
 bLength 7
 bDescriptorType 5
 bEndpointAddress 0x84 EP 4 IN
 bmAttributes 3
 Transfer Type Interrupt
 Synch Type None
 Usage Type Data
 wMaxPacketSize 0x0008 1x 8 bytes
 bInterval 5
 Interface Descriptor:
 bLength 9
 bDescriptorType 4
 bInterfaceNumber 3
 bAlternateSetting 0
 bNumEndpoints 2
 bInterfaceClass 10 CDC Data
 bInterfaceSubClass 0 [unknown]
 bInterfaceProtocol 0 
 iInterface 0 
 Endpoint Descriptor:
 bLength 7
 bDescriptorType 5
 bEndpointAddress 0x03 EP 3 OUT
 bmAttributes 2
 Transfer Type Bulk
 Synch Type None
 Usage Type Data
 wMaxPacketSize 0x0040 1x 64 bytes
 bInterval 0
 Endpoint Descriptor:
 bLength 7
 bDescriptorType 5
 bEndpointAddress 0x83 EP 3 IN
 bmAttributes 2
 Transfer Type Bulk
 Synch Type None
 Usage Type Data
 wMaxPacketSize 0x0040 1x 64 bytes
 bInterval 0
Device Status: 0x0001
 Self Powered

Here is the configuration extracted from lsusb.

 `lsusb -d 0483:5740 -v`

 

I have also modified the config to match the endpoint address.

VOID USBX_APP_Device_Init(VOID)
{
 /* USER CODE BEGIN USB_Device_Init_PreTreatment_0 */

 /* USER CODE END USB_Device_Init_PreTreatment_0 */

 /* USB_FS init function */
 /* Enable USB power */
 HAL_PWREx_EnableVddUSB(); MX_USB_PCD_Init();

 /* USER CODE BEGIN USB_Device_Init_PreTreatment_1 */
 /* USER CODE BEGIN EndPoint_Configuration */
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x00 , PCD_SNG_BUF, 0x14);

 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x80 , PCD_SNG_BUF, 0x54);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x81, PCD_SNG_BUF, 0x94);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x01, PCD_SNG_BUF, 0xD4);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x82, PCD_SNG_BUF, 0x114);

 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x02 , PCD_SNG_BUF, 0x154);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x83, PCD_SNG_BUF, 0x194);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x03, PCD_SNG_BUF, 0x1D4);
 HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x84, PCD_SNG_BUF, 0x214);
 /* USER CODE END EndPoint_Configuration */
 /* USER CODE END USB_Device_Init_PreTreatment_1 */

 /* Initialize and link controller HAL driver */
 ux_dcd_stm32_initialize((ULONG)USB, (ULONG)&hpcd_USB_FS);
 /* Start the USB device */
 HAL_PCD_Start(&hpcd_USB_FS);
 /* USER CODE BEGIN USB_Device_Init_PostTreatment */

 /* USER CODE END USB_Device_Init_PostTreatment */
}
ST Technical Moderator
September 6, 2024

Hi @NRedd.2 

You can get inspired with the example provided here How to implement a dual CDC ACM USB device using t... - STMicroelectronics Community though it uses ST library. 

 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
NRedd.2
NRedd.2AuthorBest answer
Associate III
September 9, 2024

Hi @FBL ,

 

Thank you for the response!

 

Here I have both the ACM's working with USBx stack.

[Sep 9 14:33] usb 1-4.2.1.1: USB disconnect, device number 16
[ +0.185932] usb 1-4.2.1.1: new full-speed USB device number 17 using xhci_hcd
[ +0.090350] usb 1-4.2.1.1: New USB device found, idVendor=0483, idProduct=5710, bcdDevice= 2.00
[ +0.000006] usb 1-4.2.1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000002] usb 1-4.2.1.1: Product: STM32 USB Device
[ +0.000002] usb 1-4.2.1.1: Manufacturer: STMicroelectronics
[ +0.000002] usb 1-4.2.1.1: SerialNumber: 000000000001
[ +5.275823] cdc_acm 1-4.2.1.1:1.0: ttyACM0: USB ACM device
[ +0.717204] cdc_acm 1-4.2.1.1:1.2: ttyACM2: USB ACM device