Skip to main content
Associate II
Apr 4, 2024 3:49 PM UTC
Question

Updating advertisement packet after waking up from standby mode (WB15CC)

Hi,

My application (WB15CC) stays most of the time in standby mode transmitting the advertainment packet. After a couple of minutes, the advertainment packet must be updated. When I try to update the packet after waking up from the standby mode, the firmware hangs on any of the GAP API routines, e.g. aci_gap_set_non_discoverable(), aci_gap_set_discoverable()  or aci_gap_update_adv_data().

I've edited the startup code by adding the CPUcontextSave and CPUcontextRestore routines, similar to the BLE_HeartRate example, to restore the CPU context when waking up from the standby mode. Indeed, the CPU is restored correctly I am able to register a new task inside the UTIL_SEQ_PostIdle() routine, however my task can't update the packet.

 

Can someone elucidate me what are the steps to update the advertisement packet when coming out of the standby mode?

 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
May 15, 2024 4:44 PM UTC

Hello @rs-dp 

To update the advertising data without stopping the advertising, I suggest you use the command ACI_GAP_UPDATE_ADV_DATA.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.