Skip to main content
TomC
Senior
Jan 31, 2021 11:17 PM UTC
Question

Unexpected triggering of HAL_UART_IRQHandler using HAL_UART_Receive_IT and HAL_UART_RxCpltCallback

Board: Nucleo-WB55

I'm attempting to continuously interrupt when data is received via UART.

The program is able to receive data when it is sent without fail, however the Rx interrupt is triggered when new data is not sent. I implement the following logic in my HAL_UART_RxCpltCallback routine:

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{
	strcpy((char*)command, (char*)UART1_rxBuffer);							
	rx_flag = 1;												
	HAL_UART_Receive_IT(&huart1, UART1_rxBuffer, 5);			
}

I call HAL_UART_Receive_IT after each complete call back so that a new receive request is ready. My methodology is clearly missing something, perhaps clearing a buffer or resetting a flag somewhere?

This topic has been closed for replies.

2 replies

TomC
TomCAuthor
Senior
Jan 31, 2021 11:47 PM UTC

Turns out this was caused by another UART that was being used triggering the same interrupt routine. I am yet to work out how to fix it. Will update.

TomC
TomCAuthor
Senior
Feb 1, 2021 10:18 PM UTC

Fixed by placing conditions in the call-back that check the UART Handle that triggered the interrupt, allowing me to execute specific logic for each UART.