Skip to main content
Visitor II
Jul 25, 2025 6:01 PM UTC
Solved

Unexpected RF emissions from STM32WBA55

Hello,

I'm building a BLE receiver using an STM32WBA55CG.

The device should only receive BLE advertising packets, never transmit, so I've put it in a "central" role. The device will be used very close to sensitive equipment, so it is very important that the radio never transmit.

Despite being configured as a central, and having not called any functions which I would expect to transmit (such as scanning), I am seeing two different RF emission events from the radio:

  1. A "chirp" as soon as the device is powered on
  2. Multiple "blips" some time later at random intervals

The "chirp" is a fairly quiet burst, which seems to rise in frequency across the 2.4-2.5GHz ISM band. I assume this is some kind of calibration/set-up, as it's always emitted as soon as HOST_BLE_Init() is called, from what I can see. This is manageable, as I can block the RF path when powering on/initialising the receiver for a few seconds, which should be sufficient to prevent this being emitted over the air.

The "blips" are more troubling. They are higher amplitude than the "chirp", and look like advertising packets (there is a peak at BLE channels 37, 38 and 39, if I'm reading my instruments correctly, which are the advertising channels). There doesn't seem to be a predictable gap between emissions - I've seen intervals of 1-5 seconds, but also around 30 seconds, and sometimes 10 minutes or more.

These packets will cause us problems, especially as the intervals are unpredictable (so I can't mitigate by strategically blocking the RF path as a work-around).

Can you help me understand what these emissions are? And is there any way to ensure that the radio never transmits?

Thanks,

Andy

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 1, 2025 12:54 PM UTC

Hello @andygoulden 

Since you're setting the node as central. The device will scan, discover and initiate a connection with the peripherals. That's why the advertising channels are presents. You may avoid that by setting the node to observer role.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Lina_DABASINSKAITE
ST Community Manager
Jul 28, 2025 10:04 AM UTC

Hello @andygoulden ,​  

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.​  

Best regards,​  

Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 1, 2025 12:54 PM UTC

Hello @andygoulden 

Since you're setting the node as central. The device will scan, discover and initiate a connection with the peripherals. That's why the advertising channels are presents. You may avoid that by setting the node to observer role.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.