Skip to main content
Associate
Oct 10, 2025 9:30 AM UTC
Question

Unexpected Power Draw on STM32WL55JC1 Custom Board with LoRaEndNode

Hello,

On a custom board based on the STM32WL55JC1, I managed to flash a version of the LoRaEndNode application. However, when I run it, I observe an unusually high power consumption of around 70 mA.

In contrast, when the board is in programming mode or when I run the PWR_Stop2_PeripheralNoRetention example, the current draw drops to about 6–7 mA, which matches the expected value based on my calculations.

I can share the schematics and code if needed, but I suspect the high current consumption is related to the firmware behavior rather than any hardware leakage or residual current on the board.

Is there a recommended way to reduce the power consumption of this application (AN5568 ?), or would it be better to start a new project from scratch? Do i need to code something in particular in stm32_lpm_if.c ?
Also, is this level of power consumption normal for the LoRaEndNode example?

Finally, I’ve noticed no significant difference between LowPowerSleepMode (Sleep mode with a 1 MHz clock) and STOP2 mode.

Thanks in advance for any insights.

Samy Haouara

 

This topic has been closed for replies.