Skip to main content
Associate
Jul 8, 2025 5:25 AM UTC
Solved

Unable to Flash STM32WLE5 Custom Board Using STM32WL55JC1 Debugger – Flash/Erase Errors

Hi everyone,

I'm currently trying to flash firmware to a custom board with STM32WLE5CCU6 MCU using the onboard debugger of a NUCLEO-WL55JC1 development board. I'm running into multiple issues and would appreciate any help.

Setup:

  • Target MCU: STM32WLE5CCU6 (custom board)
  • Debugger: Integrated ST-LINK on STM32WL55JC1 (used as programmer)
  • Tools: STM32CubeIDE(Ver 1.15.1) and STM32CubeProgrammer

Issue Summary:

  1. CubeProgrammer only connects at very low frequency (200 kHz SWD clock). Higher frequencies fail to detect the target.
  2.  Even when connected, flashing consistently fails with different errors on both IDE and Cube programmer depending on the attempt.(in all modes)
  3. . Errors observed in STM32CubeIDE:
Spoiler
Failed to execute MI command:
load ...\LoRaWAN_End_Node.elf
Error message from debugger back end:
Error finishing flash operation

4. Errors observed in STM32CubeProgrammer:

Spoiler
Error: failed to erase memory
Warning: failed to run application!
Warning: The core is kept under Reset!
Error: Start operation failed

Additional Notes:

  • I verified the SWD connections (SWDIO, SWCLK, NRST, GND).
  • The custom board powers up correctly.
  • I am using a basic firmware from STM32CubeWL .
  • Sometimes it connects, but erase or program operation fails.

I have attached the custom board schematic below.

Thanks in advance for any guidance!

Let me know if you want me to add or rephrase anything specific (e.g. schematic details, pinouts).

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 8, 2025 4:08 PM UTC

Hello @ruvaispari123gmailcom 

On Nucleo STLink-V3 boards it is no more possible to use the STLink for other board because the debug connector is not an "output" for debug (as on STLink-V2-1 boards) but an "input" for other tools than STLink to be able to debug the nucleo target.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Associate
Jul 14, 2025 10:36 AM UTC

Any update

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 8, 2025 4:08 PM UTC

Hello @ruvaispari123gmailcom 

On Nucleo STLink-V3 boards it is no more possible to use the STLink for other board because the debug connector is not an "output" for debug (as on STLink-V2-1 boards) but an "input" for other tools than STLink to be able to debug the nucleo target.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.