Skip to main content
Visitor II
Sep 3, 2025 9:32 PM UTC
Question

UFBGA Paste Stencil Recommendation

Hello,

 

I'd like to use the STM32WLE5 in an upcoming design. Looking at the datasheet, I noticed the recommendation for the BGA package is to have the stencil opening larger than the pad diameter, instead matching the ball diameter . To me this seems counterintuitive, as I would typically reduce the paste for balls <0.4mm in diameter. Can anyone help me understand this recommendation?

Thanks,

Billy

 

billymit_0-1756934944815.png

 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Sep 26, 2025 4:26 PM UTC

Hello @billymit 

A stencil opening larger than the pad diameter ensures that an adequate amount of solder paste is deposited and helps in achieving proper wetting of the solder ball to the pad. This is essential for the mechanical and electrical reliability of the joint. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.