Skip to main content
ABN
Associate III
Feb 24, 2025 1:10 PM UTC
Solved

TX power Level in BLE Advertisement

Hi all

We are using STM32WB55 for BLE application. By default, the TX power is added to AD data structure. 
Got to know that we can use this below API to remove the field from advertisement. 

ret = aci_gap_delete_ad_type(AD_TYPE_TX_POWER_LEVEL);


Is there a way to completely remove the TX power from AD structure? So, every time I start the advertisement, I don't need to explicitly remove the TX power parameter. 

ABN_0-1740402584432.png

 

This topic has been closed for replies.
Joe_Best answer
ST Technical Moderator
Mar 5, 2025 2:16 PM UTC

Hi,
As mentioned in the explanation of the ACI_GAP_SET_DISCOVERABLE function:


/**
* @brief ACI_GAP_SET_DISCOVERABLE
......
* With this command, the BLE Stack will also add automatically the following
* standard AD types:
* - AD Flags
* - TX Power Level

 So the only way to remove the TX Power from the ADV is to call the function 

aci_gap_delete_ad_type(AD_TYPE_TX_POWER_LEVEL);

 
Best Regards, 
Joé

2 replies

ABN
ABNAuthor
Associate III
Mar 5, 2025 10:36 AM UTC

Hey, @Remi QUINTIN 

Can you please provide me an answer for this?

Joe_Best answer
ST Technical Moderator
Mar 5, 2025 2:16 PM UTC

Hi,
As mentioned in the explanation of the ACI_GAP_SET_DISCOVERABLE function:


/**
* @brief ACI_GAP_SET_DISCOVERABLE
......
* With this command, the BLE Stack will also add automatically the following
* standard AD types:
* - AD Flags
* - TX Power Level

 So the only way to remove the TX Power from the ADV is to call the function 

aci_gap_delete_ad_type(AD_TYPE_TX_POWER_LEVEL);

 
Best Regards, 
Joé