Skip to main content
Associate III
Apr 22, 2025 8:47 PM UTC
Solved

Turning BLE on and off in STM32WB55

Hello.
I have problems turning BLE on and off on STM32WB55.

Many examples with BLE start with the lines

MX_APPE_Config();
MX_IPCC_Init();
MX_RF_Init();
MX_APPE_Init();

I do the same, and it turns on right away. I don't know how to initialize the sequencer and timeservers by themselves without BLE, so for now, I found a workaround. I turn it off using the RTC timer using the code the esteemed @FilipKremen provided me

static void BLE_exit()
{
	tBleStatus ret;
	if (BleApplicationContext.Device_Connection_Status != APP_BLE_IDLE)
	{
		ret = aci_gap_terminate(BleApplicationContext.BleApplicationContext_legacy.connectionHandle, 0x13);
		if (ret != BLE_STATUS_SUCCESS)
		 {
		 APP_DBG_MSG("aci_gap_terminate(), Failed \r\n\r");
		 }
		 else
		 {
		 APP_DBG_MSG("aci_gap_terminate(), Successfully \r\n\r");
		 }
	}

	ret = aci_hal_stack_reset();
	if (ret != BLE_STATUS_SUCCESS)
			 {
			 APP_DBG_MSG("aci_hal_stack_reset(), Failed \r\n\r");
			 }
			 else
			 {
			 APP_DBG_MSG("aci_hal_stack_reset(), Successfully \r\n\r");
			 }
}

Then I have buttons on the sequencer tasks, and the time server is still working, and I don't really understand how to enable Bluetooth with a button. Should I somehow reinitialize everything? But how can I not affect the logic of the sequencer and time server? I try to use this function 

appe_Tl_Init(); /* Initialize all transport layers */

from MX_APPE_Init in the button handler, but nothing happens, and sometimes it even hits the error handler.

Also, maybe there is a more correct way to initialize the sequencer and timeserver without initializing the BLE? How should it be turned on correctly, then?

Also, I wonder how good the idea of ​​using a sequencer and timeserver is for processing the logic of buttons and LEDs? I think that's what it was intended for?

I would be extremely grateful for your help.

 

This topic has been closed for replies.
FilipKremen
FilipKremenBest answer
ST Employee
Apr 28, 2025 1:07 PM UTC

Hello,

you can do it by not calling the appe_Tl_Init() function in MX_APPE_init().

Please note, if you're first time enabling BLE, the appe_Tl_Init() function should be called without SHCI_C2_Reinit().

Once the CPU2 is running and the second time you will be enabling BLE, call the SHCI_C2_Reinit() function before appe_Tl_Init().

 

Best regards,

ST support

7 replies

FilipKremen
ST Employee
Apr 23, 2025 7:46 AM UTC

Hello,

can you please describe more in detail what are you trying to achieve in your project?

Thank you.

 

Best regards,

Filip Kremen

 

IlliaGxAuthor
Associate III
Apr 24, 2025 11:28 AM UTC

Hello
Thank you very much for your reply
I am trying to make the logic work like this: I turn on the device with a button (it does some work unrelated to the BLE, but it works in conjunction with the sequencer and the timeserver, which handles buttons and LEDs and triggering tasks with a timer), then I can press another button and the BLE turns on. Then I can turn off the BLE using the same button (or turn off the entire device using the on/off button). So I have two buttons, one to turn the device on/off and the other to turn the BLE on/off. Let me know if I misunderstood the question.

FilipKremen
ST Employee
Apr 25, 2025 10:56 AM UTC

Hello,

if you want to enable BLE again, please try to call SHCI_C2_Reinit() function before appe_Tl_Init().

 

Best regards,

ST support

IlliaGxAuthor
Associate III
Apr 25, 2025 5:08 PM UTC

Hello,
It helped to enable BLE again, thank you. Is there a correct way to prevent BLE from turning on when starting the device? Would it be correct to call the function to disable BLE at the end of APPE_SysUserEvtRx, as you suggested in the neighboring thread, or is there another more correct approach?

 

FilipKremen
FilipKremenBest answer
ST Employee
Apr 28, 2025 1:07 PM UTC

Hello,

you can do it by not calling the appe_Tl_Init() function in MX_APPE_init().

Please note, if you're first time enabling BLE, the appe_Tl_Init() function should be called without SHCI_C2_Reinit().

Once the CPU2 is running and the second time you will be enabling BLE, call the SHCI_C2_Reinit() function before appe_Tl_Init().

 

Best regards,

ST support

IlliaGxAuthor
Associate III
Apr 29, 2025 6:46 PM UTC

Thank you very much! You are a savior in this section of the forum.