Skip to main content
Visitor II
Mar 6, 2025 2:53 PM UTC
Question

Thread time sync using WB55

Hello all,
 
I am trying to use the time sync service from openThread, using a P-NUCLEO-WB55. For that purpose, I am using the sample Thread_FTD_Coap_Multicast that is working properly. I am using the latest stm32wb5x_Thread_FTD_fw.bin image for the wireless co-processor.
 
To test the time sync, I call otNetworkTimeSetSyncPeriod on the current thread instance before enabling the thread service:
 
error = otNetworkTimeSetSyncPeriod(instance, 30);
if (error != OT_ERROR_NONE) {
APP_THREAD_Error(ERR_THREAD_START, error);
}
error = otIp6SetEnabled(NULL, true);
if (error != OT_ERROR_NONE) {
APP_THREAD_Error(ERR_THREAD_IPV6_ENABLE, error);
}
error = otThreadSetEnabled(NULL, true);
if (error != OT_ERROR_NONE) {
APP_THREAD_Error(ERR_THREAD_START, error);
 
The issue is that otNetworkTimeSetSyncPeriod is returning 126, that is not even a known otError. Also the device does not seem to be sending any sync packets as a router. Is there any known issue with the time sync implementation, or am I doing something wrong?
 
 
 
Kind regards and thanks in advance

 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Apr 4, 2025 9:01 AM UTC

Hello @maldini15 

As you said this is not a known error. Could you please try to call this function will thread protocols are disabled.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.