Skip to main content
Associate
May 24, 2024 3:37 AM UTC
Solved

The Shutdown Current is Fluctuating [shutdown的电流是波动的 ]

Hi,

The chip I am using is STM32WB55RGV6. I put it into shutdown mode and tested its current. I am using instrument room N6705C for power supply, with a voltage set to 3.3V for testing. The test result is an average current chamber of a few nA, but the waveform of the current is fluctuating, and the maximum current will look like 5uA. Is this normal?What should the current waveform look like in a normal shutdown mode?

It can be confirmed that there are basically no external connections to the IO port, and they are all configured in analog mode. I am using an inductor of 2.2uH.

Thanks.

你好,

我是用的芯片是STM32WB55RGV6,我让它进入shutdown模式并且测试了它的的电流。我是用的仪器室N6705C,使用它供电,电压设置为3.3V测试。测试结果就是平均的电流室几nA,但是电流的波形是跳动的,最大电流会有5uA样子,这是正常的吗?正常的shutdown模式的电流波形应该是什么样子的呢?

可以确定的是IO口基本没有外部的连接,都配置成了模拟状态,我是用的电感是2.2uH。

img_v3_02b4_0084192a-a1a4-421f-8498-a2e7b764c38g.jpg

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 24, 2024 6:05 PM UTC

Hello @YUNLEI 

I think this is due to the noise coming from the power supplier. 

Bets Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 24, 2024 6:05 PM UTC

Hello @YUNLEI 

I think this is due to the noise coming from the power supplier. 

Bets Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
YUNLEIAuthor
Associate
May 25, 2024 9:30 AM UTC

Hi,

Thans for you reply,

I'm sorry, I just accidentally clicked the resolved button.

You think is the noise which is form the power supplier, can you provide a specific introduction.I have tested the nucleu board MB1355D which has this issue also.

Thanks

STTwo-32
ST Technical Moderator
May 25, 2024 9:39 AM UTC

Hello @YUNLEI 

Could you try using a power supply with a very reduced Noise. I think that should solve the issue.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.