Skip to main content
User1655833706281357277
Associate III
Sep 1, 2026 7:57 PM UTC
Solved

The PWR_Exit functions for STANDBY/OFF in stm32_lpm_if.c are just placeholders and are never called on the STM32WB, right?

From the documentation it sounds like the STM32WB vectors to the reset hander when it exits STANDBY and lower power modes, correct?

 

OuadiBest answer
ST Technical Moderator
Sep 29, 2026 10:00 AM UTC

Hi ​@User1655833706281357277,

 

You are right, If the device genuinely enters Standby and a wake-up source later fires, the STM32WB does a full core reset — execution restarts at the reset vector.

 

Best regards,

Ouadi

1 reply

OuadiBest answer
ST Technical Moderator
Sep 29, 2026 10:00 AM UTC

Hi ​@User1655833706281357277,

 

You are right, If the device genuinely enters Standby and a wake-up source later fires, the STM32WB does a full core reset — execution restarts at the reset vector.

 

Best regards,

Ouadi