Question
The NUCELO-WL55JC2 433MHz transmission is greatly attenuated with LPO, but works at range with HPO. Is that a known issue?
In my testing, I programmed two NUCELO-WL55JC2's to communicate with one another. I found that I could only receive if the transmitter antenna was aligned and touching the receiving antenna.
After further debugging, I traced the issue to the LPO.
Using the low power output (even at +15dBm), gave greatly attentuated transmissions. The two antennas had to be touching.
On the other hand, using the high power output (even at only +14dBm), I could transmit at range.
Have I missed a setting for transmission? My process was based on RM0461.