Skip to main content
DS.4
Senior
Oct 12, 2021 8:53 AM UTC
Question

The effect of advertising packet data on the connection packet data

How is the advertising data :

tBleStatus aci_gap_set_discoverable( uint8_t Advertising_Type,
 uint16_t Advertising_Interval_Min,
 uint16_t Advertising_Interval_Max,
 uint8_t Own_Address_Type,
 uint8_t Advertising_Filter_Policy,
 uint8_t Local_Name_Length,
 const uint8_t* Local_Name,
 uint8_t Service_Uuid_length,
 const uint8_t* Service_Uuid_List,
 uint16_t Slave_Conn_Interval_Min,
 uint16_t Slave_Conn_Interval_Max )
{

affects the connection data:

typedef PACKED(struct)
{
 uint8_t Status;
 uint16_t Connection_Handle;
 uint8_t Role;
 uint8_t Peer_Address_Type;
 uint8_t Peer_Address[6];
 uint16_t Conn_Interval;
 uint16_t Conn_Latency;
 uint16_t Supervision_Timeout;
 uint8_t Master_Clock_Accuracy;
} hci_le_connection_complete_event_rp0;

I am looking for something that I change in the advertising packet that will cause a change in the connection complete packet.

Thanks!

This topic has been closed for replies.