Skip to main content
Associate
Dec 14, 2024 12:44 PM UTC
Question

The BLE composite HID device failed to enumerate!

 

Hello,

Recently, I have been working with the SensorTile module (STEVAL-STLCS01V1) featuring the STM32L476JG and BlueNRG-MS. I successfully created standalone HID devices for both keyboard and mouse. However, when I attempted to implement a composite HID device, the computer failed to recognize it properly.

I would like to know if BLE supports HID composite devices.

Could you provide some guidance or suggest possible solutions? Thank you!

 

I will paste my hid_report_map below.

 

 

 

 

/* USER CODE BEGIN PV */
#define FEATURE_SUPPORT_MULTIMEDIA_KEYBOARD 1 //composite hid
#define use_mouse 1
#define use_keybord 1

#if FEATURE_SUPPORT_MULTIMEDIA_KEYBOARD
#define HIDS_KB_REPORT_ID 0x01 //0x01
#define HIDS_MM_KB_REPORT_ID 0x02
#endif

static uint8_t hid_report_map[] =
{
 
#if use_keybord
	0x05, 0x01, // USAGE_PAGE (Generic Desktop)
 0x09, 0x06, // USAGE (Keyboard)
 0xa1, 0x01, // COLLECTION (Application)
#if FEATURE_SUPPORT_MULTIMEDIA_KEYBOARD //composite hid
// 0x85, HIDS_KB_REPORT_ID, // REPORT_ID (1) 
#endif
	 0x05, 0x07, // USAGE_PAGE (Keyboard)
 // bitmap of modifiers
 0x75, 0x01, // Report Size (1),
 0x95, 0x08, // Report Count (8),
 0x19, 0xE0, // Usage Minimum (224),
 0x29, 0xE7, // Usage Maximum (231),
 0x15, 0x00, // Logical Minimum (0),
 0x25, 0x01, // Logical Maximum (1),
 0x81, 0x02, // Input (Data, Variable, Absolute), ;Modifier byte
 
	
	 // 1 Reserved byte
 0x95, 0x01, // REPORT_COUNT (1)
 0x75, 0x08, // REPORT_SIZE (8)
 0x81, 0x01, // INPUT (Cnst,Ary,Abs)
	
	 // LEDs for num lock etc
 0x95, 0x05, // REPORT_COUNT (5)
 0x75, 0x01, // REPORT_SIZE (1)
 0x05, 0x08, // USAGE_PAGE (LEDs)

 0x19, 0x01, // USAGE_MINIMUM (Num Lock)
 0x29, 0x05, // USAGE_MAXIMUM (Kana)
 0x91, 0x02, // OUTPUT (Data,Var,Abs)
	
		// Reserved 3 bits
 0x95, 0x01, // REPORT_COUNT (1)
 0x75, 0x03, // REPORT_SIZE (3)
 0x91, 0x03, // OUTPUT (Cnst,Var,Abs)

	 /* Slots for 6 keys that can be pressed down at the same time */
 0x95, 0x06, // REPORT_COUNT (6)
 0x75, 0x08, // REPORT_SIZE (8)
 0x15, 0x00, // LOGICAL_MINIMUM (0)
 0x25, 0x65, // LOGICAL_MAXIMUM (101)
 0x05, 0x07, // USAGE_PAGE (Keyboard)
 0x19, 0x00, // USAGE_MINIMUM (Reserved (no event indicated))
 0x29, 0x65, // USAGE_MAXIMUM (Keyboard Application)
 0x81, 0x00, // INPUT (Data,Ary,Abs)
	
	0xC0, // END_COLLECTION
#endif

#if use_mouse

 0x05, 0x01, // USAGE_PAGE (Generic Desktop)
 0x09, 0x02, // USAGE (Mouse)
 0xa1, 0x01, // COLLECTION (Application)
#if FEATURE_SUPPORT_MULTIMEDIA_KEYBOARD //composite hid
 0x85, HIDS_MM_KB_REPORT_ID, // REPORT_ID (2)
#endif
 0x09, 0x01, // USAGE (Pointer) 鼠标指针的控制
 0xa1, 0x00, // COLLECTION (Physical)

 0x05, 0x09, // Usage Page (Buttons)
 0x19, 0x01, // Usage Minimum (1)
 0x29, 0x03, // Usage Maximum (3)
 0x15, 0x00, // Logical Minimum (0)
 0x25, 0x01, // Logical Maximum (1)
 0x95, 0x03, // Report Count (3) 
 0x75, 0x01, // Report Size (1) 
 0x81, 0x02, // Input(Data, Variable, Absolute); 3 button bits
 
	0x95, 0x01, // Report Count(1)
 0x75, 0x05, // Report Size(5)
 0x81, 0x03, // Input(Constant); 5 bit padding
 
	0x75, 0x08, // Report Size (8)
 0x95, 0x03, // Report Count (3)
 0x05, 0x01, // Usage Page (Generic Desktop)
 0x09, 0x30, // Usage (X)
 0x09, 0x31, // Usage (Y)
 0x09, 0x38, // Usage (Wheel)
 0x15, 0x81, // Logical Minimum (-127)
 0x25, 0x7F, // Logical Maximum (127)
 0x81, 0x06, // Input(Data, Variable, Relative); 3 position bytes (X,Y,Wheel)

 0xc0, // END_COLLECTION
 0xc0 // END_COLLECTION

#endif

};

 

 

 

 

 

 

This topic has been closed for replies.

1 reply

hanyangAuthor
Associate
Dec 14, 2024 1:07 PM UTC

539fcfb9c42c9b899d1372402a8a310.png

This is the packet captured on Wireshark.

I hope it do help.