Skip to main content
Associate
Sep 26, 2024 1:23 PM UTC
Solved

Test software for RF test specified in AN5796 - STM32WL Series RF Bench

Hello,

I would like to perform a LoRa Radio tests described in AN5796 - STM32WL Series RF Bench, but I do not find the needed files. So could you please share a link to firmware(STM32WL...) and software(python script and RSSMBV100 waveform).

Thanks

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 26, 2024 3:18 PM UTC

Hello @DuckTape12 and welcome to the ST Community

For the Python script, you can find it on the attachment file.

For the Firmware it is the LoRaWAN_AT_Slave that you should be using. It is available on the STM32CubeWL.

For the RF instruments, we are using the R&S®FSV signal and spectrum analyzer | Rohde & Schwarz (rohde-schwarz.com) as Spectrum analyzer and the R&S®SMBV100B vector signal generator | Rohde & Schwarz (rohde-schwarz.com) as Signal generator.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 26, 2024 3:18 PM UTC

Hello @DuckTape12 and welcome to the ST Community

For the Python script, you can find it on the attachment file.

For the Firmware it is the LoRaWAN_AT_Slave that you should be using. It is available on the STM32CubeWL.

For the RF instruments, we are using the R&S®FSV signal and spectrum analyzer | Rohde & Schwarz (rohde-schwarz.com) as Spectrum analyzer and the R&S®SMBV100B vector signal generator | Rohde & Schwarz (rohde-schwarz.com) as Signal generator.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Sep 27, 2024 8:00 AM UTC

Thanks for the reply and provided files!