Skip to main content
GScha.1
Associate
Nov 18, 2024 8:57 AM UTC
Solved

TCXO on STM32WL33

Hello,

 

I would like to know if it possible to use a 48MHz TCXO instead of the 48Mhz crystal specified in the datasheet of the STM32WL33 ?

Standard crystal are at minimum +/- 10ppm at tolerance and this may not be sufficient for our application.

 

If yes, do I left the OSC_OUTPUT in floating ?

 

Best regards,

 

Schaeffer G.

 

 

This topic has been closed for replies.
Uwe Bonnes
Uwe BonnesBest answer
Chief
Nov 18, 2024 9:18 AM UTC

Of course it is possible. But you need to enable LSE bypass. Read the docs how to do so. Osc_OUTPUT can be reused, with the restriction of the PC13-15 restrictions.

1 reply

Uwe Bonnes
Uwe BonnesBest answer
Chief
Nov 18, 2024 9:18 AM UTC

Of course it is possible. But you need to enable LSE bypass. Read the docs how to do so. Osc_OUTPUT can be reused, with the restriction of the PC13-15 restrictions.